earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concepto

Concepto


Productos MP-C, MP-V, RP-C
Funcionalidades: Hardware
Versión del producto: 3.0, 3.1, 3.2
13/05/2019

SmartX IP Controller Supported Building Standards

One of the cornerstones of the EcoStruxure BMS is support for open standards. As a result, the SmartX IP controller complies with the BACnet open standard, one of the most popular standards for buildings.

The SmartX IP controller can natively communicate with BACnet/IP networks. When the SmartX IP controller is part of an EcoStruxure BMS, the BACnet protocol is used for communication between the device and its parent EcoStruxure BMS server and other BACnet devices on the IP network, including SmartX IP controllers. As a native BACnet/IP device, the SmartX IP controller supports BACnet services such as trends, schedules, and alarms, and the controller can communicate with other BACnet devices on a BACnet/IP network. The SmartX IP controller conforms to the BACnet Advanced Application Controller (B-AAC) device profile.

  • Hardware Overview
  • MP-Cs
  • MP-Vs
  • RP-Cs