earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Commission, IP-IO , MP-C, MP-V, RP-C
Functionalities: Engineering, BACnet/IP devices
Product version: 3.3
7/17/2021

Configure Controllers with the Configuration Menu Workflow

You download an Application Image that contains a Configuration Menu to a BACnet/IP controller to configure a device. Use this workflow to implement the Configuration Menu using the eCommission SmartX Controllers mobile application. Related information can be found in the section after the flowchart.

 
action_zoom_plus_stroke Configure controllers with the eCommission application workflow
Figure: Configure controllers with the eCommission application workflow
Transfer the Application Image

Transfer the Application Image to your mobile device or Windows 10 laptop.

For more information, see Transferring an Application Image File .

Connect to the controller

In the eCommission application, connect to the controller.

For more information, see Connecting to a Device through WiFi .

For more information, see Connecting to a Controller through Bluetooth .

Download the Application Image

Download the Application Image to the BACnet/IP controller.

For more information, see Downloading an Image File to a BACnet/IP Controller .

Download the Configuration Menu to the controller

Download the Configuration Menu to the BACnet/IP controller.

For more information, see Downloading a Configuration Menu to a BACnet/IP Controller .

Modify the property values

View the property values and modify them if needed.

For more information, see Modifying Device Properties from the Configuration Menu .

  • Configuration Menu
  • Transferring an Application Image File
  • Connecting to a Device through WiFi
  • Connecting to a Controller through Bluetooth
  • Downloading an Image File to a BACnet/IP Controller
  • Downloading a Configuration Menu to a BACnet/IP Controller
  • Modifying Device Properties from the Configuration Menu