earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Poradnik

Poradnik


Produkty: eCommission SmartX Controllers, IP-IO , MP-C, MP-V, RP-C
Funkcje: Inżynieria, Urządzenia SmartX IP Controller
Wersja produktu: 2022, 2023, 2024, 7.0
2021-12-17

Connecting to Network of BACnet/IP Controllers through WiFi Router

Using a WiFi router containing a DHCP server, you can temporarily set up a WiFi network to wirelessly connect the Commission mobile application to the BACnet/IP controller network.

Pokaż więcej
action_close

Use this workflow to connect the Commission mobile application to BACnet/IP controllers.

Related information can be found in the sections that follow the flowchart.

 
action_zoom_plus_stroke Commission mobile application connection workflow
Rysunek: Commission mobile application connection workflow
Download, install, and log on to the Commission mobile application

Download, install, and log on to the Commission mobile application, and then accept the Terms of use agreement.

Więcej informacji zawiera Logging on to the Commission Mobile Application .

Power up the controllers

Power up the BACnet/IP controllers.

Więcej informacji zawiera Powering Up MP-C .

Więcej informacji zawiera Powering Up MP-V .

Prepare a wired or wireless connection for Commission mobile application

Prepare a wired or wireless connection for use with the Commission mobile application mobile device.

Connection Type

More Information

Wired connection to a single controller

Więcej informacji zawiera Connecting to Single BACnet/IP Controller by Wire .

Wired connection to a network of controllers

Więcej informacji zawiera Connecting to Network of BACnet/IP Controllers by Wire .

Wireless connection to a network of controllers via a WiFi router

Więcej informacji zawiera Connecting to Network of BACnet/IP Controllers through WiFi Router .

Wireless connection to a network of controllers via a wireless access point

Więcej informacji zawiera Connecting to Network of BACnet/IP Controllers through a Wireless Access Point .

Start the Commission mobile application and discover controllers

Start the Commission mobile application and then discover the BACnet/IP controllers on the network.

Więcej informacji zawiera Logging on to the Commission Mobile Application .

To connect to a network of BACnet/IP controllers through the WiFi Router
  1. Configure the DHCP server on the WiFi router as needed, including a suitable IP address range.

  2. Configure the network settings on the mobile device running the Commission mobile application to connect to the WiFi router.

  3. On the mobile device, enable WiFi and then connect to the wireless network.

  4. In the Commission mobile application, on the Select Connection view, select the WiFi icon

     
    action_zoom_plus_stroke
    to start wireless networking.

  5. In the Device List view, select the BACnet/IP controllers to make the connection.

Using the Commission mobile application, you can now perform tasks on the connected BACnet/IP controllers as needed.

  • Connection Workflow for the Commission Mobile Application
  • Cannot Connect Using Mobile Device with Data Plan