earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Commission, IP-IO , MP-C, MP-V
Functionalities: Engineering
Product version: 2.0, 2.1
3/14/2019

Viewing Status Information

Using the Status Information function of the eCommission SmartX Controllers mobile application, you can view status information associated with a SmartX IP controller.

Show More
action_close

The eCommission SmartX Controllers mobile application allows you to use a mobile device to perform commissioning, flow balance, and checkout operations on SmartX IP controllers. The eCommission application is available for Android and iOS (Apple) phones and tablets, as well as devices using Microsoft Windows 10. The eCommission app can connect to a single SmartX IP controller or to a network of SmartX IP controllers on the local network.

User Roles and Functions

The eCommission application provides a portable, simplified user interface to access SmartX IP controllers without the need to use a dedicated workstation or portable computer. The eCommission app is activated for one of three roles:

  • Technician: Commissions and maintains the configuration of a building system containing SmartX IP controllers

  • Electrician: Physically installs and wires the devices in a system containing SmartX IP controllers

  • Flow Balancer: Flow balances a VAV unit controlled by a SmartX MP-V controller

Each of these roles is assigned permissions appropriate to the user's unique functions and responsibilities. The main menu of the eCommission app, when activated for a Technician, lists five major functions and three additional functions. A ninth function, the Controller List Creator, can be accessed after logging in to the app, in the Select Connection view. The following tables summarize the association between the user roles and these major and additional functions.

Major functions

Table: User Roles and Associated Major Functions

Applicable

User Roles

Major Functions

Technician

Device Settings

You can configure many of the device settings in SmartX IP controllers using the eCommission mobile application. You can also configure network communications settings shared by a selection of multiple SmartX IP controllers.

For more information, see SmartX IP Controller Device Settings .

Technician

Flow Balancer

Flow Balance

Used to air balance terminal boxes controlled by SmartX MP-V controllers. This function automates most of the air balance procedure but it also allows you to manipulate VAV tasks individually.

For more information, see Flow Balance Overview .

Technician

Electrician

I/O Checkout

After you have wired the physical inputs and outputs of the controller, you can perform I/O checkout to verify that the wiring was done correctly and that the physical inputs and outputs are working properly. The I/O checkout status of each input and output can be found in the Inputs and Outputs view. In the Device List view, the checkout statuses of all the inputs and outputs in a SmartX IP Controller device are aggregated and displayed as the Checkout status of the controller.

As you are performing I/O checkout, two files are generated in the background, within the SmartX IP Controller device. An I/O checkout report details the results of the checkout, and a commissioning log file records the steps that were performed. At the completion of checkout these files can be viewed in WorkStation.

For more information, see Performing I/O Checkout .

Technician

Browse Objects

Once aSmartX IP controller is installed and checked out, you can use the Browse Objects function of the eCommission SmartX Controllers mobile application to view and edit the objects within a controller.

For more information, see Browsing and Modifying Object Properties .

Technician

Electrician

Status Information

You can use the Status Information function of the eCommission SmartX Controllers mobile application to view status information associated with a SmartX IP controller. This information includes the BACnet ID of the controller's device object, the controller's model name and serial number, the version of firmware and software in the controller, and the host server name and ID.

For more information, see Viewing Status Information .

Technician

Electrician

Flow Balancer

Controller List Creator

The Controller List Creator of the eCommission SmartX Controllers mobile application can be used when documenting the SmartX IP Controller devices on an EcoStruxure network. The Controller List Creator captures device information from the Data Matrix symbol on the tear-off product info label of a SmartX IP Controller device, largely automating this process. In turn, the captured information can be exported to a comma-separated file for use as system documentation.

For more information, see Using Controller List Creator .

Additional functions

Table: User Roles and Associated Additional Functions

Applicable

User Roles

Additional Functions

Technician

Electrician

Download Image : Download an application image to a SmartX IP controller

For more information, see Downloading an Application Image to SmartX IP Controller .

Technician

Electrician

Diagnostic Files : View and export diagnostic files from within a SmartX IP controller

For more information, see Diagnostic Files .

Technician

Electrician

Device Restart : Perform a warm or cold restart of a SmartX IP controller

For more information, see Device Restart .

Supported Platforms

The eCommission application supports the following platforms:

  • Android 6.0 (Marshmallow) and later

  • Apple iOS 11.2 and later

  • Microsoft Windows 10

Help Resources in the eCommission Application

The eCommission SmartX Controllers mobile application contains video and text-based help resources designed to introduce the user to its principal functions and features, and as a quick reference for the workflow associated with the Technician, Electrician, or Flow Balancer role.

Video tutorials

A series of short video tutorials describe how you can use the various functions in the eCommission application to perform tasks on SmartX IP Controller devices. You can find a list of these tutorials by tapping the Help icon

 
action_zoom_plus_stroke
within the application. Internet access is required when viewing these video tutorials.

Help articles

The eCommission application also includes context-sensitive help articles about its key features and functions. When you are performing a task with the eCommission application, you can tap the Help icon

 
action_zoom_plus_stroke
in that view to open an article explaining the feature or function.

To view status information
  1. In the Device List view, select the SmartX IP controller in which you want to view the status information and then tap NEXT .

    Note:

    The Device List view has filters that allow you to easily find and select the controller:

    • If you are logged in as a Flow Balancer, the device list is automatically filtered to show only MP-V controllers.

    • If you are logged in as a Technician or Electrician, you can sort the list of discovered devices by controller model.

  2. In the Device Settings view, tap the Menu button

     
    action_zoom_plus_stroke
    .

  3. Tap Status Information to view status information associated with the controller.

  4. In the Status Information view, review the status information.

You have viewed the current status information from the controller.

  • eCommission SmartX Controllers Mobile Application Overview