SmartX Sensor LCD Temperature Sensor Model- Heating and Cooling Mode Screen
Use the SmartX Sensor LCD Temperature Sensor model Heating and Cooling Mode screen to view and configure the current heating or cooling setting.
action_zoom_plus_stroke
Figure:
SmartX Sensor LCD Temperature Sensor Model - heating and cooling mode screen
Table: SmartX Sensor LCD Temperature Sensor Model- Heating and Cooling Mode Screen
|
Component
|
Description
|
action_zoom_plus_stroke
|
Identifies the screen as the heating and cooling mode screen.
|
|
Heating and cooling mode setting
|
Displays whether heating or cooling mode is in operation:
You can change heating and cooling mode settings using the interface buttons.
For more information, see SmartX Sensor LCD Temperature Sensor Model- Default Screen
.
For more information, see Changing Heating and Cooling Mode Settings
.
|
SmartX Sensor LCD Temperature Sensor Model
SmartX Sensor LCD Temperature Sensor Model- Default Screen
SmartX Sensor LCD Temperature Sensor Model- Home Screen
SmartX Sensor LCD Temperature Sensor Model- Fan Speed Screen
SmartX Sensor LCD Temperature Sensor Model- Degree Type Screen
SmartX Sensor LCD Temperature Sensor Model- Occupancy Mode Screen
Changing the Temperature Setpoint
Changing the Fan Speed
Changing Heating and Cooling Mode Settings
Changing the Occupancy Mode
Changing the Degree Type