SmartX Sensor LCD Temperature Sensor Model- Occupancy Mode Screen
Use the SmartX Sensor LCD Temperature Sensor model Occupancy mode screen to view and configure the room occupancy mode.
action_zoom_plus_stroke
Figure:
SmartX Sensor LCD Temperature Sensor Model - occupancy mode screen
Table: SmartX Sensor LCD Temperature Sensor Model- Occupancy Mode Screen
|
Component
|
Description
|
action_zoom_plus_stroke
|
Identifies the screen as the occupancy mode screen.
|
|
Occupancy mode setting
|
Displays the curent setting indicating whether the room is occupied or unoccupied:
Yes: Occupied
No: Unoccupied
You can change the occupancy mode setting to tell the control system that the room is occupied or unoccupied using the interface buttons.
For more information, see SmartX Sensor LCD Temperature Sensor Model- Default Screen
.
For more information, see Changing the Degree Type
.
|
SmartX Sensor LCD Temperature Sensor Model
SmartX Sensor LCD Temperature Sensor Model- Default Screen
SmartX Sensor LCD Temperature Sensor Model- Home Screen
SmartX Sensor LCD Temperature Sensor Model- Fan Speed Screen
SmartX Sensor LCD Temperature Sensor Model- Heating and Cooling Mode Screen
SmartX Sensor LCD Temperature Sensor Model- Degree Type Screen
Changing the Temperature Setpoint
Changing the Fan Speed
Changing Heating and Cooling Mode Settings
Changing the Occupancy Mode
Changing the Degree Type