earth_america
user_standard Accedi
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Modalità

Modalità


Prodotti: eCommission SmartX Controllers, IP-IO , MP-C, MP-V, RP-C
Funzionalità: Ingegneria, Impostazioni SmartX IP Controller
Versione del prodotto: 3.0, 3.1, 3.2, 3.3
12/08/2019
Clicca per visualizzare la versione aggiornata non ancora tradotta

Gestione dei progetti in Creatore elenco dispositivi

Nella vista Elenco progetti della funzione Creatore elenco dispositivi , puoi visualizzare i progetti esistenti ed eliminarli o crearne di nuovi.

Mostra di più
action_close

The eCommission SmartX Controllers mobile application allows you to use a mobile device to perform commissioning, flow balance, and checkout operations on SpaceLogic BACnet/IP devices. BACnet/IP devices include BACnet/IP controllers (MP and RP) and IP-IO modules. The eCommission application is available for Android and iOS (Apple) phones and tablets, as well as devices using Microsoft Windows 10. The eCommission app can connect to a single BACnet/IP device or to a network of BACnet/IP devices on the local network.

Preparations

Prior to using the eCommission SmartX Controllers mobile application at a job site, there are some preparations you must make to facilitate device commissioning.

Per maggior informazioni, consulta Preparations .

Device Connection

The eCommission SmartX Controllers application supports device connection through BACnet Wi-Fi and wireless Bluetooth connection.

Per maggior informazioni, consulta Device Connection .

Bluetooth Adapter

The SpaceLogic Bluetooth Adapter allows you to establish a Bluetooth connection to MP controllers. You plug the Bluetooth Adapter into the corresponding SpaceLogic Sensor to connect to the controller.

Per maggior informazioni, consulta SpaceLogic Bluetooth Adapter .

Device Settings

The Device Settings view of the eCommission SmartX Controllers mobile application allows you to configure most of the settings of the BACnet/IP controller. You can save a particular device settings configuration to a Common Settings file. Common Device Settings files can be downloaded to multiple BACnet/IP controllers to facilitate device configuration.

Per maggior informazioni, consulta BACnet/IP Controller Device Settings .

Image Downloading

Image files are created by a WorkStation user and contain pre-engineered objects, properties, and values. Download an Image to a BACnet/IP controller to facilitate device commissioning tasks.

Per maggior informazioni, consulta Image Downloading .

Configuration Menu

Configuration Menus are a group of pre-engineered objects and values that make device commissioning faster and easier. Configuration Menus are exported and downloaded from image files. Download a Configuration Menu to a BACnet/IP controller to commission the controller.

Per maggior informazioni, consulta Configuration Menu .

I/O Checkout

After you have wired the physical inputs and outputs of the controller, you perform I/O checkout to verify that the wiring was done correctly and that the physical inputs and outputs are working properly.

Per maggior informazioni, consulta I/O Checkout Overview .

Flow Balancing

The Flow Balance function of the eCommission SmartX Controllers mobile application is used to air balance terminal boxes controlled by MP-V controllers. This function automates most of the air balance procedure but it also allows you to manually check out the flow balance by driving the damper to a specified position, a flow setpoint, or a flow value.

Per maggior informazioni, consulta Bilanciamento flusso .

Device Restart

Use the Device Restart function of the eCommission SmartX Controllers application to perform a restart of the BACnet/IP controller. There are four different ways to restart the BACnet/IP controller.

Per maggior informazioni, consulta Device Restart .

Gestire i progetti in Creatore elenchi di controllori
  1. In Creatore elenchi di controllori , nella vista Creatore elenco , seleziona il pulsante Gestione file

     
    action_zoom_plus_stroke
    nella parte superiore della finestra.

  2. Nella vista Elenco progetti , rivedi l'elenco dei progetti esistenti creati con l'applicazione eCommission.

  3. Scegli se eliminare un progetto o crearne uno nuovo:

    • Per eliminare un progetto, seleziona il progetto dall'elenco e quindi seleziona Cancella .

    • Per creare un nuovo progetto, seleziona Nuovo quindi segui il processo di creazione di un nuovo progetto.

      Per maggior informazioni, consulta Capturing a Device with the Controller List Creator .

  4. Una volta terminato, seleziona Continua per tornare alla vista Creatore elenco .

Hai esaminato l'elenco dei progetti e cancellato progetti o ne hai creato uno nuovo.

  • eCommission SmartX Controllers Mobile Application Overview
  • Capturing a Device with the Controller List Creator