earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Hur göra

Hur göra


Produkter: eCommission SmartX Controllers, IP-IO , MP-C, MP-V, RP-C
Funktionaliteter: Maskinteknik, SmartX IP-kontrollenheter
Produktversion: 2022, 2023, 2024, 7.0
2025-02-13

Connecting to Single BACnet/IP Controller by Wire

Running the Commission mobile application on a Windows laptop computer, you can connect directly to a BACnet/IP controller by Ethernet wire. Optionally, you can use an Ethernet switch to connect the computer and the BACnet/IP controller.

Visa mer
action_close

Use this workflow to connect the Commission mobile application to BACnet/IP controllers.

Related information can be found in the sections that follow the flowchart.

 
action_zoom_plus_stroke Commission mobile application connection workflow
Figur: Commission mobile application connection workflow
Download, install, and log on to the Commission mobile application

Download, install, and log on to the Commission mobile application, and then accept the Terms of use agreement.

Mer information finns i Logging on to the Commission Mobile Application .

Power up the controllers

Power up the BACnet/IP controllers.

Mer information finns i Powering Up MP-C .

Mer information finns i Powering Up MP-V .

Mer information finns i Powering Up an RP-V Controller .

Prepare a wired or wireless connection for Commission mobile application

Prepare a wired or wireless connection for use with the Commission mobile application mobile device.

Connection Type

More Information

Wired connection to a single controller

Mer information finns i Connecting to Single BACnet/IP Controller by Wire .

Wired connection to a network of controllers

Mer information finns i Connecting to Network of BACnet/IP Controllers by Wire .

Wireless connection to a network of controllers via a WiFi router

Mer information finns i Connecting to Network of BACnet/IP Controllers through WiFi Router .

Wireless connection to a network of controllers via a wireless access point

Mer information finns i Connecting to Network of BACnet/IP Controllers through a Wireless Access Point .

Start the Commission mobile application and discover controllers

Start the Commission mobile application and then discover the BACnet/IP controllers on the network.

Mer information finns i Logging on to the Commission Mobile Application .

To connect to a single BACnet/IP controller by wire
  1. Configure the network connections on the Commission mobile application computer and the BACnet/IP controller for DHCP addressing.

    Mer information finns i Configuring BACnet/IP Controller Settings .

  2. Connect an Ethernet cable between the Commission mobile application computer and Port 1 of the BACnet/IP controller. If you are using an Ethernet switch, connect the computer and the controller to the switch, using Ethernet cables.

    Obs!

    Because an actual DHCP server is not used, both the Commission mobile application computer and the BACnet/IP controller will self-assign link-local IP addresses.

  3. In the Commission mobile application, on the Home page, click IP Network , select a network adapter, and discover devices.

  4. In the Device List view, select the BACnet/IP controller to make the connection.

Using the Commission mobile application, you can now perform tasks on the connected BACnet/IP controller as needed.

  • Connection Workflow for the Commission Mobile Application
  • Configuring BACnet/IP Controller Settings