earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WebStation
Functionalities: Dashboards
Product version: 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024
2/23/2024

Configuring a Heat Map

You configure a heat map to get a graphical representation of data where the individual values contained in a matrix are represented as colors.

Show More
action_close

A heat map is a graphical representation of data where the values contained in a matrix are represented as colors.

Heat map is typically used to present a trend log. A Heat map can be used to display any information, for example temperature, water consumption, or energy consumption.

The color and scale of the blocks in the Heat map can be changed to fit its content. For example, cooling can be displayed in various blue shades and heating in various yellow and red shades.

To configure a heat map
  1. Click Configure or click the Settings button

     
    action_zoom_plus_stroke
    .

  2. In the Heat Map Properties dialog box, in the Display trend log box, enter the trend log you want to display as a heat map.

  3. In the Period box, select a period.

  4. In the Calculation method box, select a calculation method.

  5. In the Caption box, type a caption.

  6. In the Caption link box, enter a link to an object that is relevant for the heat map.

  7. In the Show Legend box, select True to display the name and color of the trend log in the heat map.

  8. Click Add to add a guide to define the colors for different values and value ranges.

  9. In the Value box, select a value for the guide.

  10. In the Color box, select a color for the value or value range.

  11. In the Decimal box, select the number of decimals to display.

  12. Click OK .

  • How Dashboards Work
  • Dashboard Widgets
  • Heat Map
  • Heat Map Properties Dialog Box
  • Adding a Widget to a Dashboard