earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: WebStation
功能: Dashboards
产品版本: 2024, 7.0
2024/12/3

Configuring a Period over Period Chart

You configure a period over period chart so that you can compare trend logs over different time periods.

显示更多
action_close

Dashboard widgets are small applications in a dashboard. Dashboard widgets are the main components in a dashboard and present graphical information from your system.

您可在仪表板中创建一个或多个仪表板小部件。只能在 WebStation 中的仪表板中创建仪表板小部件。

准备好供使用

所有仪表板小部件已准备好供使用。您唯一需要做的就是添加趋势日志、变量、警报或要在仪表板小部件中显示的事件。所有仪表板都具有默认的颜色设置和不同的部件组件,但是也可对它们进行配置以符合自己的需求。例如,您可向小部件本身添加标题或者在图表中添加 x 和 y 轴,您可对测量仪中的不同值或值范围使用不同的颜色。

克隆小部件和重新绑定小部件引用

You can clone widgets and rebind widgets references.

有关更多信息,请参阅 Clone Widgets and Rebind Widget References .

空处

空处并非仪表板小部件,但是属于在仪表板小部件之间创建空处的一种方式。在您处理仪表板的布局时,会用到空处。

警报计数

An alarm count displays the number of alarms from the EcoStruxure Building Operation system.

有关更多信息,请参阅 Alarm Count .

警报帕累托图

An alarm Pareto chart is a graphical representation of alarms represented by bars but also by a cumulative line. An alarm pareto chart gives you a quick overview of the most common causes of alarms.

有关更多信息,请参阅 Alarm Pareto Chart .

警报饼图

An alarm pie chart is a circular graphic divided into slices to illustrate proportions of alarms.

有关更多信息,请参阅 Alarm Pie .

警报桑基图

An alarm Sankey chart is used to graphically present a Sankey chart of the alarms in the EcoStruxure Building Operation system.

有关更多信息,请参阅 Alarm Sankey Chart .

事件帕累托图

An event Pareto chart is a graphical representation where the events are represented by bars but also by a cumulative line. An event pareto chart gives you a quick overview of the most common events.

有关更多信息,请参阅 Event Pareto Chart .

事件饼图

An event pie chart is a circular graphic divided into slices to illustrate proportions of events.

有关更多信息,请参阅 事件饼图 .

事件发生率图

An event rate chart is a graphical representation of event rates represented by bars.

有关更多信息,请参阅 Event Rate Chart .

事件桑基图

An events Sankey chart is used to graphically present a Sankey chart of the events in the EcoStruxure Building Operation system.

有关更多信息,请参阅 Event Sankey Chart .

热图

A heat map is a graphical representation of data where the values contained in a matrix are represented as colors.

有关更多信息,请参阅 Heat Map .

图片小部件

An image widget displays an image in a dashboard.

有关更多信息,请参阅 图片小部件 .

日志测量仪

A log gauge displays trend log values in a gauge.

有关更多信息,请参阅 Log Gauge .

日志饼

A log pie chart is a circular graphic divided into slices to illustrate proportions of trend logs.

有关更多信息,请参阅 Log Pie .

记录值

A log value displays one or many trend log values as numerical values.

有关更多信息,请参阅 Log Value .

周期图

A period chart is used to compare trend logs over different time periods.

有关更多信息,请参阅 Period Chart .

周期图表

A period chart is used to compare trend logs over different time periods.

有关更多信息,请参阅 Period over Period Chart .

点测量仪

A point gauge is used to graphically display a current value in a gauge.

有关更多信息,请参阅 Point Gauge .

点饼

A point pie chart is a circular graphic divided into slices to illustrate proportion of values.

有关更多信息,请参阅 Point Pie .

点值

A point value is used to display the present value of one or many variables as a numerical value.

有关更多信息,请参阅 Point Value .

XY 绘图

A XY plot, also called a scatter plot, is used to display values for two trend logs.

有关更多信息,请参阅 XY Plot .

浏览

使用“浏览”导航至您要添加至仪表板的图形或超链接。

动态仪表板小工具

Dynamic widgets is a way to automatically add graphics to a dashboard using a search function.

有关更多信息,请参阅 Dynamic Widgets .

图形

Graphics can be added to a dashboard.

有关更多信息,请参阅 Graphics in Dashboards .

超链接

也可将超链接添加至仪表板。要能够显示超链接的内容,必须让外部内容能够嵌入 WebStation。

有关更多信息,请参阅 Configuring Security in WebStation using WorkStation .

To configure a period over period chart
  1. Click Configure or click the Settings button

     
    action_zoom_plus_stroke
    .

  2. Click Add .

  3. Select the trend logs and click Select .

  4. In the Chart type box, select how the trend log is displayed.

  5. In the Calculation method box, select a calculation method for the trend chart.

  6. In the Color box, enter a color for the trend log.

  7. Select the position of the Y-axis.

  8. I the Missing data list, select how to handle missing data in the chart.

  9. In the Period box, select a period.

  10. In the Caption box, type a caption.

  11. In the Caption Link box, enter a link to an object that is relevant for the period over period chart.

  12. In the Show Legend box, select True to display the name and color of the trend log in the period over period chart.

  13. In the Show Period box, select True to display the period as a legend.

  14. In the Stack series , select True to stack the series bars.

  15. In Y-axis minimum box, enter the minimum value of the left y-axis.

  16. In Y-axis maximum box, enter the maximum value of the left y-axis.

  17. In the Decimal box, select the number of decimals.

  18. Click OK .

  • How Dashboards Work
  • 仪表板小部件
  • Period over Period Chart
  • Period over Period Chart Properties – Dialog Box
  • Adding a Widget to a Dashboard