Dashboard widgets are small applications in a dashboard. Dashboard widgets are the main components in a dashboard and present graphical information from your system.
You can create one or many dashboard widgets in a dashboard. Dashboard widgets can only be created in a dashboard in WebStation.
Ready to use
All dashboard widgets are ready to use. The only thing you have to do is add the trend log or variable you want to display in the dashboard widget. All dashboard widgets have default setting for color and different layout components, but you can also configure them to suit your needs. For example, you can add captions to the widget itself or the x- and y-axis in diagram, you can use different colors for different values or value ranges in a gauge.
Empty Space
Empty space is not a dashboard widget but a way to create empty spaces between dashboard widgets. Empty spaces are used when you do the layout of a dashboard.
Heat Map
A heat map is a graphical representation of data where the values contained in a matrix are represented as colors.
Mer information finns i Heat Map
.
Log Gauge
A log gauge displays trend log values in a gauge.
Mer information finns i Log Gauge
.
Log Pie
A log pie chart is a circular graphic divided into slices to illustrate proportions of trend logs.
Mer information finns i Log Pie
.
Log Value
A log value displays one or many trend log values as numerical values.
Mer information finns i Log Value
.
Period Chart
A period chart is used to compare trend logs over different time periods.
Mer information finns i Period Chart
.
Period over Period Chart
A period chart is used to compare trend logs over different time periods.
Mer information finns i Period over Period Chart
.
Point Gauge
A point gauge is used to graphically display a current value in a gauge.
Mer information finns i Point Gauge
.
Point Pie
A point pie chart is a circular graphic divided into slices to illustrate proportion of values.
Mer information finns i Point Pie
.
Point Value
A point value is used to display the present value of one or many variables as a numerical value.
Mer information finns i Point Value
.
XY Plot
A XY plot, also called a scatter plot, is used to display values for two trend logs.
Mer information finns i XY Plot
.
Browse
Use Browse to navigate to a graphic or a hyperlink that you want to add to a dashboard.