You configure a XY plot to display correlation between trend logs.
Click Configure or click the Settings button
In the X-Axis Log box, enter the log you want to display on the X-axis.
In the X-Axis Calculation box, select the calculation method for the X-Axis.
In the Y-Axis Log box, enter the log you want to display on the Y-axis.
In the Y-Axis Calculation box, select the calculation method for the Y-Axis.
In the Period box, select a period.
In the Calculation period box, select a calculation period.
Select Scatter to display all values as individual points in the diagram.
Select Contour to display a contour map of the correlation of values.
Select Gridlines to display gridlines in the diagram.
Select Linear Regression Line to display the values as a linear regression line.
Select Polynominal Regression Curve to display the values as a polynomial regression line.
In the Caption box, type a caption.
In the Caption link box, enter a link to an object that is relevant for the point gauge.
In the Show Period box, select True to display the period as a legend.
In the X-Axis Caption box, enter a caption for the X-axis.
In the Y-Axis Caption box, enter a caption for the Y-axis.
In the Point color box, enter the color for the points in the diagram.
In the Inner Contour Color box, enter the inner color for a contour map in the diagram.
In the Outer Contour Color box enter the outer color for a contour map in the diagram.
In the Line Color box, enter the color for a linear regression line in the diagram.
In the X-axis minimum box, enter the minimum value of the x-axis.
In the X-axis maximum box, enter the maxium value of the left x-axis.
In the Y-axis minimum box, enter the minimum value of the y-axis.
In the Y-axis maximum box, enter the maximum value of the y-axis.
In the Decimal box, select the number of decimals to display.
Click OK .