earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-B, Edge Server, Device Administrator, ​License Administrator, AS-P
功能: 硬件, SmartDriver
产品版本: 2023
2022/12/16

Automation Server Licensing on Automation Servers Connected to Internet Workflow

Use this workflow to add licenses to automation servers with access to Internet.

Related information can be found in the sections after the flowchart.

 
action_zoom_plus_stroke Automation server licensing workflow
图: Automation server licensing workflow
Install certificates on the automation servers

Install certificates if you use HTTPS for communication.

有关更多信息,请参阅 Device Administrator Certificate Workflow .

Entitlements

Make sure that you have the Entitlements containing the licenses. You need the email with the entitlement during the process.

Make sure that the automation servers have access to Internet

The Automation servers must have access to Internet for the activation process.

有关更多信息,请参阅 Information Technology System Planning Guide .

Add an entitlement in Device Administrator

In Device Administrator, you add entitlements that contains products and licenses.

This is done so that you can view all licenses that are available to be assigned and then activated.

Make sure that you have the HTML entitlement certificate file or the entitlement ID available .

There are two different procedures to add and set up an entitlement when you have an automation server connected to internet:

Assign licenses to an automation server

Use the License Products available in the entitlements to assign License Features to the automation servers.

有关更多信息,请参阅 Assigning Licenses .

Activate licenses on an automation server

有关更多信息,请参阅 Activating Licenses Online .

  • Automation Server Licensing Overview
  • Information Technology System Planning Guide
  • Adding an Entitlement using the HTML file when Automation Server is Connected to License Server (FNO)
  • Adding an Entitlement without the HTML file when Automation Server is Connected to License Server (FNO)
  • Assigning Licenses
  • Activating Licenses Online
  • Automation Server Licensing on Automation Servers not Connected to Internet Workflow
  • Automation Server Licensing on Automation Servers not Connected to Internet Workflow