earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-B, Edge Server, Device Administrator, AS-P
功能: 硬件, 许可证管理
产品版本: 2023
2023/4/12

Automation Server Licensing on Automation Servers not Connected to Internet Workflow

Use this workflow to assign and activate licenses on automation servers that do not have any access to Internet.

Related information can be found in the sections after the flowchart.

 
action_zoom_plus_stroke Assign and activate licenses on automations servers without Internet access workflow
图: Assign and activate licenses on automations servers without Internet access workflow
Install certificates on the automation servers

Install certificates if you use HTTPS for communication.

有关更多信息,请参阅 Device Administrator Certificate Workflow .

Entitlements

Make sure that you have the Entitlements containing the licenses. You need the email with the entitlement during the process.

有关更多信息,请参阅 Order Information Request .

Add an entitlement in Device Administrator

In Device Administrator, you add entitlements that contains products and licenses.

This is done so that you can view all licenses that are available to be assigned and then activated.

Make sure that you have the HTML entitlement certificate file or the entitlement ID available .

There are two different procedures to add and set up an entitlement:

Assign licenses to automation servers

Use the License Products available in the entitlements to assign License Features to the automation servers.

有关更多信息,请参阅 Assigning Licenses .

Create the request files

In Device Administrator, create the request files.

有关更多信息,请参阅 Creating the Request Files .

Activate request files on License Activation Server (FNO) to receive response files

Using Device Administrator, activate request files on License Activation Server (FNO) to receive response files. To be able to complete this procedure, you must be on a computer that is connected to License Activation Server (FNO) via the Internet and have Device Administrator installed.

有关更多信息,请参阅 Activating Request Files to Receive Response Files .

Send response files to the automation servers

Using Device Administrator, send the response files to the automation server to complete the license activation.

有关更多信息,请参阅 Sending the Response Files to the Automation Server .

Backup the automation server

After the licenses has been installed, make a backup of the automation server to make sure that you do not lose the licenses if any problems occur.

有关更多信息,请参阅 Backup .

  • Activating Request Files to Receive Response Files
  • Creating the Request Files
  • Activate Licenses Dialog Box
  • Sending the Response Files to the Automation Server
  • Backup
  • Assigning Licenses
  • Automation Server Licensing on Automation Servers not Connected to Internet Workflow
  • Automation Server Licensing on Automation Servers Connected to Internet Workflow