earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Device Administrator, AS-P
功能: 硬件, 许可证管理
产品版本: 2023
2022/12/17

Adding an Entitlement using the HTML file when Automation Server is Connected to License Server (FNO)

You add the entitlement to view the License Products available for activation on automation servers.

显示更多
action_close

Device Administrator is used to manage licenses on automation servers.

Software and Features that Require Licenses

A number of software features need licenses.

有关更多信息,请参阅 Software and Features that Require Licenses .

Entitlements, Products, and Licenses

Licenses are bought as products and delivered in Entitlements. An Entitlement is a container that can contain several products. The products contain the licenses and they can differ in quantity and contents.

Automation Server Licensing Workflow

Use one of these workflows, depending on if the automation servers are connected or not connected to the Internet.

有关更多信息,请参阅 Automation Server Licensing on Automation Servers Connected to Internet Workflow .

有关更多信息,请参阅 Automation Server Licensing on Automation Servers not Connected to Internet Workflow .

Certificates

It is recommended to use HTTPS for the communication between Device Administrator and automation servers when you manage licenses.

有关更多信息,请参阅 Certificates Managed using Device Administrator .

Return Licenses on SpaceLogic Automation Servers

You can return licenses from automation servers.

有关更多信息,请参阅 Return Licenses on SpaceLogic Automation Servers .

To add an entitlement using the HTML file when automation server is connected to License Server (FNO)
  1. In Device Administrator, click Entitlements .

  2. Click Add Entitlement or click from Entitlement Certificate File .

  3. Click Browse and select the HTML entitlement certificate file.

  4. Click Next .

  5. Click Add .

  • Automation Server Licensing Overview
  • Order Information Request
  • Licenses Activation Server
  • Add and Setup Entitlement
  • Assign Licenses View
  • Assigning Licenses
  • Activating Licenses Online
  • Adding an Entitlement without the HTML file when Automation Server is Connected to License Server (FNO)
  • Automation Server Licensing on Automation Servers Connected to Internet Workflow
  • Automation Server Licensing on Automation Servers not Connected to Internet Workflow