Use this workflow to add licenses to SmartX servers using Device Administrator.
Related information can be found in the sections after the flowchart.
action_zoom_plus_stroke
Figure:
SmartX Serverr licensing workflow
Add Entitlements to Device Administrator
In Device Administrator, add an Entitlement that contains products and licenses to Device Administrator.
For more information, see Adding an Entitlement to Device Administrator
.
Assign licenses to a SmartX server
Assign the licenses in the Entitlement for the features you want to use on the SmartX servers.
For more information, see Assigning Licenses
.
Activate licenses on a SmartX server
For more information, see Activating Licenses Online
.
If you do not have internet access, you can activate licenses offline.
For more information, see Offline Activation of Licenses Workflow
.
Important:
Activated licenses cannot be deactivated.