earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
3
Concept

Concept


Products: AS-B, Device Administrator, AS-P
Functionalities: Hardware, License Management
Product version: 3.3
2/21/2022

Offline Activation of Licenses Workflow

Use this workflow to activate licenses offline. Offline activation is typically used when Device Administrator and the automation servers are not connected to the Internet. Related information can be found in the sections after the flowchart.

 
action_zoom_plus_stroke Offline activation of licenses workflow
Figure: Offline activation of licenses workflow
Create the request files

In Device Administrator, create the request files.

For more information, see Creating the Request Files .

Activate request files on License Activation Server (FNO) to receive response files

Using Device Administrator, activate request files on License Activation Server (FNO) to receive response files. To be able to complete this procedure, you must be on a computer that is connected to License Activation Server (FNO) via the Internet, and have Device Administrator installed.

For more information, see Activating Request Files to Receive Response Files .

Send response files to the automation servers

Using Device Administrator, send the response files to the automation server to complete the license activation.

For more information, see Sending the Response Files to the Automation Server .

Backup the automation server

After the licenses has been installed, make a backup of the automation server to make sure that you do not lose the licenses if the automation server crashes.

For more information, see Backup .

  • Automation Server Licensing Overview
  • Activating Request Files to Receive Response Files
  • Creating the Request Files
  • Activate Licenses Dialog Box
  • Sending the Response Files to the Automation Server
  • Backup