earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: AS-B, Edge Server, Device Administrator, AS-P
Functionalities: Hardware, License Management
Product version: 2023
12/16/2022

Activating Request Files to Receive Response Files

You activate request files on License Activation Server (FNO) to receive response files. To be able to complete this procedure, you must be on a computer that is connected to the Internet and have Device Administrator installed.

Show More
action_close

Device Administrator is used to manage licenses on automation servers.

Software and Features that Require Licenses

A number of software features need licenses.

For more information, see Software and Features that Require Licenses .

Entitlements, Products, and Licenses

Licenses are bought as products and delivered in Entitlements. An Entitlement is a container that can contain several products. The products contain the licenses and they can differ in quantity and contents.

Automation Server Licensing Workflow

Use one of these workflows, depending on if the automation servers are connected or not connected to the Internet.

For more information, see Automation Server Licensing on Automation Servers Connected to Internet Workflow .

For more information, see Automation Server Licensing on Automation Servers not Connected to Internet Workflow .

Certificates

It is recommended to use HTTPS for the communication between Device Administrator and automation servers when you manage licenses.

For more information, see Certificates Managed using Device Administrator .

Return Licenses on SpaceLogic Automation Servers

You can return licenses from automation servers.

For more information, see Return Licenses on SpaceLogic Automation Servers .

To activate request files to receive response files
  1. In Device Administrator, click Servers .

  2. Select Show Licenses .

  3. Click Activate licenses .

  4. Click Offline Step 2 - Activate request files on License Activation Server (FNO) to receive response files.

  5. Click OK .

  6. In the Select the zip file containing the request files you want to activate box, select the request file.

  7. Enter the password for the request file.

  8. In the Select the name and location of the zip file that will contain the response file, select a name and a location for the response file.

    The default location and name of the Response file is the same as the Request file.

  9. Click Activate .

  10. Click Close .

  • Automation Server Licensing Overview
  • Automation Server Licensing on Automation Servers not Connected to Internet Workflow
  • Creating the Request Files
  • Sending the Response Files to the Automation Server