earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: AS-B, Edge Server, Device Administrator, AS-P
Functionalities: Hardware, License Management
Product version: 2023
12/16/2022

Sending the Response Files to the Automation Server

You send the response files to the automation servers to complete the offline activation of licenses. The computer is connected to the automation servers but not connected to Internet.

Show More
action_close

Device Administrator is used to manage licenses on automation servers.

Software and Features that Require Licenses

A number of software features need licenses.

For more information, see Software and Features that Require Licenses .

Entitlements, Products, and Licenses

Licenses are bought as products and delivered in Entitlements. An Entitlement is a container that can contain several products. The products contain the licenses and they can differ in quantity and contents.

Automation Server Licensing Workflow

Use one of these workflows, depending on if the automation servers are connected or not connected to the Internet.

For more information, see Automation Server Licensing on Automation Servers Connected to Internet Workflow .

For more information, see Automation Server Licensing on Automation Servers not Connected to Internet Workflow .

Certificates

It is recommended to use HTTPS for the communication between Device Administrator and automation servers when you manage licenses.

For more information, see Certificates Managed using Device Administrator .

Return Licenses on SpaceLogic Automation Servers

You can return licenses from automation servers.

For more information, see Return Licenses on SpaceLogic Automation Servers .

To send response files to the Automation server
  1. In Device Administrator, click Servers .

  2. Select Show licenses .

  3. Select the automation servers.

  4. Click Offline Step 3 - Send response files to the selected automation server s.

  5. Click OK .

  6. In the Select the zip file that contains the response files you want to send , select the response files.

  7. Click Send .

  • Automation Server Licensing Overview
  • Automation Server Licensing on Automation Servers not Connected to Internet Workflow
  • Send Response Files to Automation Servers Dialog Box
  • Creating the Request Files
  • Activating Request Files to Receive Response Files