earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-L, AS-B, Device Administrator, AS-P
功能: 硬件, 许可证管理
产品版本: 3.0, 3.1
2019/5/13

Sending the Response Files to the SmartX Server

You send the request files to the SmartX servers to complete the offline activation of licenses.

显示更多
action_close

Device Administrator is used to manage licenses on SmartX server.

Licenses on SmartX Servers

Licenses are needed with some of the features of a SmartX server.

SmartDrivers

To be able to use SmartDrivers on a SmartX server, one or more, license is needed for every SmartDriver that runs on the SmartX server.

SNMP Notifications

To be able to use SNMP Notification on a SmartX server, a license is required.

One license for SNMP Notifications allows you to use any number of SNMP Notifications on that SmartX server.

Personal Dashboards

To be able to create personal dashboards on a SmartX server, you need a license. Personal dashboards are used in WebStation.

One license allows the connected users of that SmartX server to create any number of Personal Dashboards.

Entitlements, Products, and Licenses

Licenses are bought as products and delivered in Entitlements. An Entitlement is a container that can contain several products. The products contain the licenses and they can differ in quantity and contents.

有关更多信息,请参阅 Entitlements, Products, and Licenses .

Assign and Activate Licenses

When you have added the Entitlement to Device Administrator you must assign and activate the licenses.

有关更多信息,请参阅 Assign and Activate Licenses .

Certificates

It is recommended to use HTTPS for the communication between Device Administrator and SmartX servers when you manage licenses.

有关更多信息,请参阅 Certificates in Device Administrator .

重要:

Activated licenses cannot be deactivated.

To send response files to the SmartX server
  1. In Device Administrator, click Servers .

  2. Select Show licenses .

  3. Select the SmartX servers.

  4. Click Send response files .

  5. In the Select Response file dialog box, click Select folder .

  6. Browse to the response files.

  7. Click OK .

All assigned licenses are now activated.

  • Device Administrator Licenses
  • Offline Activation of Licenses Workflow
  • Offline Response Files Dialog Box
  • Creating the Request Files
  • Uploading the Request Files and Downloading the Response Files