earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Commission, IP-IO , MP-C, MP-V, RP-C
Functionalities: Engineering, BACnet/IP devices
Product version: 3.1, 3.2
12/19/2019

Modifying Device Properties from the Configuration Menu

After downloading the configuration menu to the controller, you view and modify the device properties from the configuration menu to complete device commissioning.

Show More
action_close

Configuration Menus are a group of pre-engineered objects and values that make device commissioning faster and easier. Configuration Menus are exported and downloaded from image files. Download a Configuration Menu to a SmartX IP Controller to commission the controller.

Configure Controllers Workflow

You download an Application Image that contains a Configuration Menu to a SmartX IP controller to configure a device. Use this workflow to implement the Configuration Menu using the eCommission SmartX Controllers mobile application. Related information can be found in the section after the flowchart.

For more information, see Configure Controllers with the Configuration Menu Workflow .

Download a Configuration Menu to a SmartX IP Controller

You download the Configuration Menu to the SmartX IP controller to configure the device.

For more information, see Downloading a Configuration Menu to a SmartX IP Controller .

Modify Device Properties from the Configuration Menu

After downloading the configuration menu to the controller, you view and modify the device properties from the configuration menu to complete device commissioning.

For more information, see Modifying Device Properties from the Configuration Menu .

To modify device properties from the configuration menu
  1. From the Menu , select Configuration Menu .

  2. In the Configuration Menu, change any writable property values.

  3. Select Save .

  4. To verify a change in value, select the Refresh icon. Property values refresh when you navigate to and from submenus.

You have completed device commissioning for this controller and can continue performing device configuration on other SmartX IP controllers.

  • Configuration Menu