You download the Configuration Menu to the SmartX IP controller to configure the device.
Before you can download a Configuration Menu to a SmartX IP Controller, you must download the Application Image that contains the Configuration Menu to the SmartX IP Controller. For more information, see Downloading an Image File to a SmartX IP Controller .
From the Menu , select Configuration Menu .
In the Configuration Menu, change any writable property values. For more information, see Modifying Device Properties from the Configuration Menu .
Select Save .
The Configuration Menu has been downloaded to the SmartX IP Controller.