earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-B, Enterprise Server, AS-P, Project Configuration Tool, RP-C, RP-C-EXT-0-10V-4-PD, RP-C-EXT-BL-2-LV-PD, RP-C-EXT-BL-4-HV-PD, RP-C-EXT-DALI-M-PD, RP-C-EXT-MS-BLE
功能: 工程, 硬件
产品版本: 3.1, 3.2
2019/12/28

RP Series Expansion Module and Multi-sensor Memory

RP Series expansion modules and multi-sensor have two types of memory, flash memory and RAM.

The flash memory is used as follows:

  • Embedded flash memory: for boot loader, operating system, application software, and configuration storage

  • NOR flash memory: for log files and default configuration storage

The RAM is used for runtime operation.

The configuration data for the RP Series expansion modules and multi-sensors resides in the RP-C controller to which the devices are connected. When the RP-C controller is part of an EcoStruxure BMS, the configuration data for the controller, expansion modules, and multi-sensors automatically resides in the parent EcoStruxure BMS server. Any configuration changes made through the EcoStruxure Building Operation software are stored in the EcoStruxure BMS server as well as the hosted RP-C controller and its subsystem. This means there is always a backup available for restoring or replacing an RP-C controller.

注释:

Configuration changes made through a third party BACnet Operator Workstation (B-OWS) or the eCommission SmartX Controllers mobile application are not automatically part of the configuration data in the EcoStruxure BMS server. You need to upload such configuration changes if you want the changes to be stored in the EcoStruxure BMS server.

Scheduled backups of the EcoStruxure BMS server can provide additional protection against application and data loss. You can also manually back up or restore an EcoStruxure BMS server to a storage location on a PC or network.  

  • RP Series Expansion Modules and Multi-sensors
  • Light Modules
  • Blind Modules
  • RP-C-EXT-DALI-M-PD
  • RP-C-EXT-0-10V-4-PD
  • RP-C-EXT-BL-4-HV-PD
  • RP-C-EXT-BL-2-LV-PD
  • RP-C-EXT-MS-BLE
  • SmartX IP Controller - RP Series Models
  • RP-Cs
  • SmartX IP Controller Device Firmware Management
  • Free Object System Memory Utilization in SmartX IP Controllers
  • Application Images
  • SmartX IP Controller Communication
  • Association Selection Workflow
  • Configure an Online SmartX IP Controller Workflow
  • SmartX IP Controller Diagnostics
  • Device Discovery for SmartX IP Controller Devices
  • SmartX IP Controller Device Management
  • Automatic Time Sync for SmartX IP Controllers
  • BACnet Backup and Restore