The RP controller expansion blind modules enable control of motorized window blinds and shutters.
The blind modules support blind motors that operate on AC mains voltage (230 VAC) as well as DC motors (24 VDC). The blind modules also come in different models that support blind motor drives with Standard Motor Interface (SMI) as well as conventional motor drives.
Module |
Blind Motor |
SMI-interface |
RP-C-EXT-BL-SMI-4-HV-PD |
230 VAC |
yes |
RP-C-EXT-BL-SMI-2-LV-PD |
24 VDC |
yes |
RP-C-EXT-BL-4-HV-PD |
230 VAC |
no |
RP-C-EXT-BL-2-LV-PD |
24 VDC |
no |
The RP-C-EXT-BL-SMI-4-HV-PD SMI blind module connects to the RP-C room controllers and provides I/O expansion for control of AC mains-supplied motors (drives) with SMI (Standard Motor Interface for AC applications).
有关更多信息,请参阅 RP-C-EXT-BL-SMI-4-HV-PD .
The RP-C-EXT-BL-SMI-2-LV-PD SMI blind module connects to the RP-C room controllers and provides I/O expansion for control of DC low-voltage motors (drives) with SMI LoVo (Standard Motor Interface for low-voltage applications).
有关更多信息,请参阅 RP-C-EXT-BL-SMI-2-LV-PD .
The RP-C-EXT-BL-4-HV-PD blind module connects to the RP-C room controllers and provides I/O expansion for high-voltage blind control.
有关更多信息,请参阅 RP-C-EXT-BL-4-HV-PD .
The RP-C-EXT-BL-2-LV-PD blind module connects to the RP-C room controllers and provides I/O expansion for low-voltage blind control.
有关更多信息,请参阅 RP-C-EXT-BL-2-LV-PD .