earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Automation Server, AS-B, Enterprise Central, Enterprise Server, AS-P
Functionalities: User Management
Product version: 3.1
12/19/2019

Setting an EcoStruxure BMS Server to Password Reset Mode

You set an EcoStruxure BMS server to password reset mode so that you can create a new password if the old one was forgotten.

Show More
action_close

You can reset the administrator password on your EcoStruxure Building Operation servers. Related information can be found in the sections after the flowchart.

 
action_zoom_plus_stroke Password Reset Workflow
Figure: Password Reset Workflow
Set the server in password reset mode

In Device Administrator, set the Enterprise Server, Enterprise Central and SmartX server in reset mode.

For more information, see Setting an EcoStruxure BMS Server to Password Reset Mode .

In Project Configuration Tool, set the Project Configuration Tool server in reset mode.

For more information, see Setting an EcoStruxure PCT Server to Password Reset Mode .

Copy the session ID

In WorkStation, copy the session ID that you need to get a temporary password.

For more information, see Copying the Session ID when Resetting the Password .

Send the session ID to Schneider Electric Buildings support team

Contact your local Schneider Electric Buildings support team and send them the session ID.

Create a new password

Log on to the server using the temporary password supplied by Schneider Electric Buildings support team and create the new password.

For more information, see Resetting the Password using WorkStation .

Note:

To set an Enterprise Server or Enterprise Central to password reset mode, the servers must run on the same computer as Device Administrator. You must also add the Enterprise Server or Enterprise Central manually. For more information, see Connecting to an Enterprise Server or Enterprise Central .

To set a SmartX server to password reset mode, you must be connected using the USB port. For more information, see Connecting to a SmartX Server Using the USB Device Port .

To set an EcoStruxure BMS Server in password reset mode
  1. In Device Administrator, click Servers and then click the EcoStruxure BMS Server name.

  2. Click Password Reset .

  3. In the Password reset token dialog box, click OK .

The EcoStruxure Building Operation server is now in password reset mode for 24 hours.

  • Password Reset Workflow
  • Connecting to a SmartX Server Using the USB Device Port
  • Connecting to a SmartX Server Using the IP Network
  • Copying the Session ID when Resetting the Password