earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Basic Functionality
Product version: 3.2, 3.3, 2022
2/3/2021

Property Context Menu

Use the property context menu to open the menu specific for the given property from the properties list.

 
action_zoom_plus_stroke Property context menu
Figure: Property context menu

Table: Property Context Menu

Command

Description

New

​Click to open the New submenu where you create new objects.

Select unit...

Click to open the Select Unit dialog box. For more information, see Select Unit Dialog Box .

Select retain level...

Click to open the Select Retain Level dialog box.

Copy

​Click to copy the selected objects. The objects are placed on the clipboard.

  • Property Context Menu
  • Property Context Menu – New Submenu