Use the New submenu to create new objects.
Command |
Description |
Alarm |
Click to open the Create Object wizard where you create an alarm. For more information, see Create Object Dialog – Naming the Object Page . An alarm monitors a variable and alerts you if the monitored variable matches the configured alarm conditions. For more information, see Alarms Overview . |
Trend |
Click to open the Create Object wizard where you create trend logs, trend log lists, or trend charts. For more information, see Create Object Dialog – Naming the Object Page . The function of a trend log is to log the variable that it is connected to and store the records. For more information, see Trends Overview . |