Our site will be unavailable from October 29-30 due to scheduled maintenance.
Thank you for your patience.
RP-C-CRS-DEMO is a demonstration kit for the Connected Room Solutions for Buildings.
The demo kit is intended to be used for demos in trade shows, trainings, and in meetings with partners, system integrators, consultants, and end customers.
The demo kit is a portable tool for demonstrating Connected Room Solution functions such as light and blind control, multi-sensor operation, and control using SpaceLogic* Sensors.
The demo kit is designed for 230 VAC (50/60 Hz) operation.
* Formerly known as SmartX
The demo kit has been designed for demonstration of the following features:
Light and blind control
Multi-sensor operation
Control using SpaceLogic Sensors
|
Product |
Part number |
|
RP-C-CRS-DEMO
|
SXWRECRSDEMO10001
|
|
Product |
Part number |
|
AS-P |
SXWASPXXX10001 |
|
PS-24V power supply to AS-P |
SXWPS24VX10001 |
|
RP-C
(RP-C-16A-F-230V)
|
SXWRCF16A10002 |
|
DALI light module
(RP-C-EXT-DALI-M-PD)
|
SXWREDAMPD10001 |
|
Low-voltage blind module
(RP-C-EXT-BL-2-LV-PD)
|
SXWREB2LVPD10001 |
|
Multi-sensor
(RP-C-EXT-MS-BLE)
|
SXWREMSBLE10001 |
|
SpaceLogic Sensor base with temperature, humidity, and CO 2 sensors |
SXWSBTHCXSXX |
|
SpaceLogic Sensor cover with touchscreen display with light and blind control buttons |
SXWSC4XSELXW |
The demo kit also includes the following equipment:
IP67 rated case
LED light and DALI LED driver for lighting demo
LED light strip for blind position simulation
24 VDC power supply
RJ45 and USB connectors
On/Off switches
Residual current breaker with overcurrent protection
IEC power cord, USB cables, and patch cables are not included in the demo kit.
| AC input | |
Nominal voltage
|
230 VAC
|
Frequency
|
50/60 Hz
|
| Mechanical | |
Dimensions
|
638 x 505 x 224 mm (25.1 x 19.9 x 8.8 in.)
|
Weight
|
10.8 kg (23.8 lb)
|
| Software compatibility | |
EcoStruxure Building Operation software
|
version 3.2 and later
|
|
Marking |
Internal Connection |
Function/Typical Use |
|
USB/AS-P |
USB Device port on AS-P |
Configuration of IP address using Device Administrator |
|
USB/RP-C |
USB Host port on RP-C |
Reserved for future use |
|
IP1/AS-P |
Ethernet 1 port on AS-P |
Connection to Local Area Network (LAN) |
|
IP2/AS-P |
Ethernet 2 port on AS-P |
Connection to RP-C (IP1/RP-C) |
|
IP1/RP-C |
Ethernet 1 port on RP-C |
Connection to AS-P (IP2/AS-P) or to another AS-P network if used in demo of zoning |
|
IP2/RP-C |
Ethernet 2 port on RP-C |
Extension of IP network with additional RP-Cs |
|
COMA/RP-C |
RS-485 (RJ45) Com A port (“Sensor Bus”) on RP-C |
Daisy chaining of SpaceLogic Sensors (room sensors) on sensor bus |
|
COMB/RP-C |
RS-485 (RJ45) Com B port (“Room Bus”) on RP-C |
Daisy chaining of RP Series expansion modules, such as light modules, blind modules, and multi-sensors, on room bus |
|
DI1 |
Digital Input 1 (DI1) on DALI light module |
Programmable function, switch on/off control of lights |
|
DI2 |
Digital Input 2 (DI2) on DALI light module |
Programmable function, switch on/off control of lights |
|
DI3 |
Digital Input 1 (DI1) on low-voltage blind module |
Programmable function, switch on/off |
|
DI4 |
Digital Input 2 (DI2) on low-voltage blind module |
Programmable function, switch on/off |