You create a Multi schedule viewer to view and edit several schedules at the same time.
In WebStation, in the System Tree pane, right-click a schedule you want to include in the Multi schedule viewer and click Create Multi schedule viewer .
In the Name field, type a name.
In the Path field, enter the location of the Multi schedule viewer.
Click Add to add more schedules to the Multi schedule viewer.
In the Select object dialog box, do one of the following:
Click Browse to browse the system to find the schedules you want to add.
Click Object matching type , to get a list of all schedules in the system that can be added.
Select the schedules you want to add.
Click Select .
Click OK .
You can also add new schedules to the Multi schedule viewer by clicking the Add button in the Multi schedule viewer toolbar. Więcej informacji zawiera Adding a Schedule to a Multi Schedule Viewer .