earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Poradnik

Poradnik


Produkty: WebStation
Funkcje: Harmonogramy
Wersja produktu: 2022, 2023
2021-12-17

Opening a Schedule from a Multi Schedule Viewer

You can open a schedule from a Multi schedule viewer if you want to edit the schedule.

Pokaż więcej
action_close

You can create a Multi schedule viewer in WebStation to edit and view a number of schedules at the same time.

A Multi schedule viewer is useful for example if you want to add at the same events on several schedules at the same time. You can select the schedules you want to add the events on.

A Multi schedule viewer also gives you an overview of the attached schedules.

To open a schedule from a Multi Schedule Viewer
  1. In WebStation, click the Multi schedule viewer.

  2. In the Multi schedule viewer, right-click the name of the schedule you want to edit and click Open schedule .

  • Multi Schedule Viewer
  • Multi Schedule Viewer Workspace
  • Multi Schedule Viewer Toolbar
  • Creating a Multi Schedule Viewer
  • Adding a Schedule to a Multi Schedule Viewer
  • Removing a Schedule from a Multi Schedule Viewer
  • Adding the Same Event to Multiple Schedules
  • Assigning a Value on Click