earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Pojęcie

Pojęcie


Produkty: WebStation
Funkcje: Harmonogramy
Wersja produktu: 2022, 2023
2021-12-17

Multi Schedule Viewer

You can create a Multi schedule viewer in WebStation to edit and view a number of schedules at the same time.

A Multi schedule viewer is useful for example if you want to add at the same events on several schedules at the same time. You can select the schedules you want to add the events on.

A Multi schedule viewer also gives you an overview of the attached schedules.

  • How Schedules Work
  • Creating a Multi Schedule Viewer
  • Adding a Schedule to a Multi Schedule Viewer
  • Removing a Schedule from a Multi Schedule Viewer
  • Adding the Same Event to Multiple Schedules
  • Assigning a Value on Click
  • Opening a Schedule from a Multi Schedule Viewer