Funzionalità: Funzionalità di base
Versione del prodotto: 2023
20/06/2023

Backing up and Restoring using WebStation

You can backup and restore the server from WebStation.

Mostra di più
action_close

A subset of backup and restore features are available in WebStation.

You can create backups of the server using WebStation. The backup can be downloaded and uploaded from the server.

Scheduled backup must be done using WorkStation.

Per maggior informazioni, consulta Backup .

To backup and restore
  1. Click WebStation, click Workspace menu .

  2. Click System .

  3. Click Backup and restore .

  4. In the Backup and restore dialog:

    • Click Backup to create a manually initiated backup.

    • Select a backup and click Restore to restore the server to the selected backup.

  • Backup and Restore Overview
  • Backup and Restore using WebStation
  • Uploading and Downloading a Backup using WebStation
  • Backup