Funzionalità: Funzionalità di base
Versione del prodotto: 2023
20/06/2023

Uploading and Downloading a Backup using WebStation

You can upload and download a backup using WebStation.

Mostra di più
action_close

A subset of backup and restore features are available in WebStation.

You can create backups of the server using WebStation. The backup can be downloaded and uploaded from the server.

Scheduled backup must be done using WorkStation.

Per maggior informazioni, consulta Backup .

To upload and download a backup using WebStation
  1. Click WebStation, click Workspace menu .

  2. Click System .

  3. Click Backup and restore .

  4. In the Backup and restore dialog:

    • Click Upload to upload a backup.

    • Select a backup and click Download to download the selected backup.

  • Backup and Restore Overview
  • Backup and Restore using WebStation
  • Backing up and Restoring using WebStation
  • Backup