earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: AS-B, Device Administrator, AS-P
Functionalities: License Management
Product version: 2022
1/8/2025

Return Demo Licenses File from Device Administrator

You return demo licenses after they have expired or when you commission a site.

Do not remove the demo licenses file from Device Administrator until all demo licenses are removed from your automation servers.

Show More
action_close

Demo licenses are used for demonstration purposes, training, or when building a site.

There are two types of demo licenses:

  • EcoStruxure Building Operation Software Demo Licenses on Windows. These licenses are managed by License Administrator and handles licenses on Enterprise Server and Enterprise Central.

  • SpaceLogic Automation Server Demo Licenses. These licenses are managed by Device Administrator and handles licenses on Automation Servers.

EcoStruxure Building Operation Software Demo License on Windows Management

Demo licenses for EcoStruxure Building Operation software are local, bound to the computer, and cannot be shared.

The license file used to activate demo licenses can only be used once per computer and is time-limited. The demo license is installed on License Server from a license file with the extension .asr. Demo licenses must be activated on the same computer that runs WorkStation, Enterprise Server or Enterprise Central.

For more information, see EcoStruxure Building Operation Software Demo Licenses on Windows Management .

SpaceLogic Automation Server Demo License Management

You add and return licenses on automation servers using Device Administrator.

For more information, see SpaceLogic Automation Server Demo License Management .

To return a demo license file from Device Administrator
  1. In Device Administrator, click Entitlements .

  2. In the Entitlements view, click Demo License .

  3. Click Delete .

  4. Click the Save current list button

     
    action_zoom_plus_stroke
    .

The demo license is returned. You must now purchase, assign, and activate licenses for the features you want to use.

For more information, see Automation Server Licensing on Automation Servers Connected to Internet Workflow .

  • Demo Licensing Overview
  • Returning Demo Licenses from SpaceLogic Automation Servers Workflow
  • Returning Demo Licenses from SpaceLogic Automation Servers
  • Licenses View
  • Unable to Activate or Return a EcoStruxure Building Operation Software License