earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: AS-B, Device Administrator, AS-P
Functionalities: Hardware, License Management
Product version: 2022
1/8/2025

Returning Demo Licenses from SpaceLogic Automation Servers

You return demo licenses after they have expired or when you commission a site.

You cannot activate or deactivate licenses when the automation server is connected using a USB cable.

Show More
action_close

Use this workflow to return demo licenses from automation servers.

Related information can be found in the sections after the flowchart.

 
action_zoom_plus_stroke Return demo licenses from SpaceLogic automation servers workflow
Figure: Return demo licenses from SpaceLogic automation servers workflow
Return demo licenses from automation servers

Return the demo licenses from your automations servers using Device Administrator.

For more information, see Return Demo Licenses File from Device Administrator .

Do not remove the demo licenses file from Device Administrator until all demo licenses are removed from your automation servers.

Return demo licenses file from Device Administrator

When you have returned all demo licenses from your automation server you can return the demo licenses file from Device Administrator if you are not going to use them again.

For more information, see Return Demo Licenses File from Device Administrator .

To return demo licenses from SpaceLogic automation servers
  1. In Device Administrator, click Servers .

  2. Select Show licenses .

  3. In the Assign Licenses view, in the License status column, click the Show products button

     
    action_zoom_plus_stroke
    .

  4. In the Assign column, in the row for Demo , clear Assign .

  5. In the Deactivate Demo License dialog box, click Yes .

  6. Click OK .

Repeat the procedure for all other automation servers you want to return demo licenses from.

  • Demo Licensing Overview
  • Returning Demo Licenses from SpaceLogic Automation Servers Workflow
  • Return Demo Licenses File from Device Administrator
  • Assign Licenses View