earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: AS-B, Edge Server, Device Administrator, AS-P
Functionalities: Engineering, License Management
Product version: 2024
10/30/2025

Returning Licenses on Field Servers Connected to Internet

You return licenses so that they can be used elsewhere.

Show More
action_close

You can return licenses from field servers.

This is done, for example, if you for some reasons have assign and activated licenses on a field server that does not need licenses. When the licenses have been returned they can be activated and assigned on another field server.

When you return licenses, all licenses on the selected server are returned.

Consider the following cases when returning licenses on field servers.

Online

In the online case the computer that runs Device Administrator is connected to the Internet.

For more information, see Returning Licenses on Field Servers Connected to Internet .

Online return on a semi online system

A special case is semi online system where the EcoStruxure BMS server is not connected to Internet, but Devices Administrator is connected to Internet. A semi online system is treated as an online system for licensing purposes.

For more information, see Semi Online System .

For more information, see Returning Licenses on Field Servers Connected to Internet .

Offline

In the offline case the computer that runs Device Administrator and the field servers are not connected to the Internet. Neither the Device Administrator nor the field servers can connect to License Activation Sever (FNO).

Use this workflow to return licenses when neither Device Administrator nor the field servers are connected to the Internet.

For more information, see Return Licenses on Field Servers not Connected to Internet (FNO) Workflow .

To return Licenses on field servers connected to Internet
  1. In Device Administrator, click Servers .

  2. Select Show licenses .

  3. Select the field servers where you want to return the licenses.

  4. Click Return .

  5. Click Return licenses online .

  6. Click OK .

  • Field Server Licensing Overview
  • Return Licenses on Field Servers
  • Other Menu