Prodotti: AS-B, Edge Server, Device Administrator, AS-P
Funzionalità: Hardware, Gestione della licenza
Versione del prodotto: 2023
16/12/2022

Add Entitlement from File

Use the Add Entitlement from file dialog box to add the entitlement.

 
action_zoom_plus_stroke Add Entitlement from file dialog box
Figura: Add Entitlement from file dialog box

Tabella: Add Entitlement from File Dialog Box

Command

Description

Browse

Browse to the entitlement file.

  • Automation Server Licensing on Automation Servers Connected to Internet Workflow
  • Automation Server Licensing on Automation Servers not Connected to Internet Workflow
  • Restarting Automation Servers from Device Administrator
  • Add Entitlement from ID
  • Checking Entitlement Dialog Box
  • Contacting License Activation Server Dialog Box