earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: RP-V
Functionalities: Hardware
Product version: 2022, 2023, 2024, 7.0, 7.1
3/30/2023

RP-V Communication Ports

The RP controller provides a combination of communication ports, such as:

  • Ethernet port(s)

  • USB port(s)

  • RS-485 port(s)

The number and types of communication ports differ between the different controller models.

Regarding the differences in the set of communcation ports, the RP-V models can be divided into the following two categories:

  • RP-V-4A and RP-V-5A

  • Model with “-M” in the product name: RP-V-5C-M

For more information, see RP-V Models .

Communication Ports on RP-V-4A and -5A

The RP-V-4A and RP-V-5A models provide the following combination of communication ports:

  • Two Ethernet ports

  • One USB port

  • Two RS-485 ports (RJ45)

For more information, see Communication Ports on RP-V-4A and -5A .

Communication Ports on RP-V-5C-M

The RP-V-5C-M model provides the following communication ports:

  • One RS-485 port with RJ45 interface

  • One RS-485 port with terminal block

For more information, see Communication Ports on RP-V-5C-M .

  • RP-V Controllers
  • RP-V Models
  • Communication Ports on RP-V-4A and -5A
  • Communication Ports on RP-V-5C-M