The MP-C provides the following communication port:
One RS-485 port with terminal block
The RS-485 port with screw terminal block is used for connection to the BACnet MS/TP (RS-485) network.
The screw terminals are labeled:
RS-485+
RS-485–
Shield
For more information, see MP-C-24A-M Screw Terminals .
For more information, see MP-C-36A-M Screw Terminals .
For more information, see RS-485 Communications .