earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: Sustainability
产品版本: 2024, 7.0
2024/12/10

Consumption Signature – Output Consumption Tab

Use the Consumption Signature – Output consumption tab to view the consumption during a specific time period.

 
action_zoom_plus_stroke Consumption Signature – Output consumption tab
图: Consumption Signature – Output consumption tab

表格: Consumption Signature – Output Consumption Tab

Component

Description

Enable output consumption

Actual consumption

Displays the actual consumption, that is the calculated consumption from the consumption log.

Expected consumption

Displays the expected consumption, that is the expected consumption according to the signature curve.

Consumption difference

Displays the consumption difference if the consumption is higher or lower than the expected consumption.

Dependency value

Displays the dependency value, that is the calculated dependency value from the dependency log.

Period start

Period end

  • Energy Consumption Overview
  • General Information Properties – Basic Tab
  • Consumption Signature - Basic Tab
  • Consumption Signature – Input Consumption Tab
  • Consumption Signature – Output Consumption Tab
  • Consumption Signature – Expected Consumption Signature Curve Tab