earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: Sustainability
产品版本: 2024, 7.0
2024/2/23

Consumption Signature – Input Consumption Tab

Use the Consumption Signature – Input consumption tab to add logs and edit logs.

 
action_zoom_plus_stroke Consumption Signature – Input consumption tab
图: Consumption Signature – Input consumption tab

表格: Consumption Signature – Input Consumption Tab

Component

Description

Consumption log

Browse to the energy meter object that logs the actual energy consumption.

Consumption log calculation type

Select the consumption log calculation type.

有关更多信息,请参阅 Consumption Log Calculation .

Dependency log

Browse to the dependency log that affects the energy consumption.

Dependency log calculation type

Select the dependency log calculation type.

有关更多信息,请参阅 Consumption Log Calculation .

Calculation period

Select the period you want to compare and get the expected consumption for.

History period

Select the period you want to create the signature curve for.

  • Energy Consumption Overview
  • General Information Properties – Basic Tab
  • Consumption Signature - Basic Tab
  • Consumption Signature – Input Consumption Tab
  • Consumption Signature – Output Consumption Tab
  • Consumption Signature – Expected Consumption Signature Curve Tab