earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Пользовательский интерфейс

Пользовательский интерфейс


Продукты: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Функции: Sustainability
Версия продукта: 2024, 7.0
23.02.2024

Meter Object – Outputs Tab

Use the Meter Object – Outputs tab to view the output from the meter object.

 
action_zoom_plus_stroke Meter Object – Outputs tab
Рисунок: Meter Object – Outputs tab

Таблица: Meter Processor – Outputs Tab

Component

Description

Meter value (kWh)

Displays the total meter value output. Read-only.

Current hour (kWh)

Displays the consumption during the current hour. Read-only.

Current day (kWh)

Displays the consumption during the current day. Read-only.

Current week (kWh)

Displays the consumption during the current week. Read-only.

Current month (kWh)

Displays the consumption during the current month. Read-only.

Current year (kWh)

Displays the consumption during the current year. Read-only.

  • Energy Consumption Overview
  • Meter Object
  • Meter Object – Basic Tab