earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Comment faire pour

Comment faire pour


Produits : AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Fonctionnalités : Sustainability
Version produit : 2024, 7.0
23/02/2024

Finalizing a Meter Replacement

You finalize a meter replacement after you have replaced the physical meter that is monitored by the meter object. When you finalize a meter replacement, the meter object starts logging and collecting values from the physical meter.

Update the configuration of the monitored variable if the new physical meter is exposed using a different address or register.

Afficher plus
action_close

When you replace a physical meter, you need to make adjustment to the meter object that monitor the physical meter.

Meter replacement must be planned to avoid data loss.

Use this workflow to replace a meter. Pour plus d'informations, voir Meter Replacement Workflow .

To finalize a meter replacement
  1. Do one of the following:

    • In WorkStation, right-click the meter object, point to Meter management then click Finalize meter replacement .

    • In WebStation, right-click the meter object, then click Finalize meter replacement .

  2. Specify the start value and the maximum value for the new meter in the dialog box.

  3. Click OK .

  • Meter Replacement
  • Meter Replacement Workflow
  • Initiating a Meter Replacement
  • Finalizing a Meter Replacement