earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Sustainability
Product version: 2024, 7.0
2/23/2024

Viewing a Meter Processor Chart

You view a graphical representation of your meter processor to better understand the energy consumption.

Show More
action_close

The meter processor object is used to process the information from one or many meter objects. Using the meter processor, you can add or subtract energy consumption from many different meter objects. A meter processor can also process information from another meter processor.

Meter Processor Charts

You can display a chart in WebStation that shows how much each connected meter object, or meter processor, contributes to the calculated result.

For more information, see Meter Processor Charts .

Suppressed Reduction

The meter processor has a built-in mechanism to avoid negative consumption.

For more information, see Meter Processor Suppressed Reduction .

Meter Object Data Migration in Meter Processor

There are three ways to handle data migration when you create a meter processor.

  • No migration

  • Migration from the newest meter start time

  • Migration from the oldest meter log start time

For more information, see Meter Object Data Migration in Meter Processor .

To view a meter processor chart
  1. In WebStation, click the meter processor.

  2. In the meter processor menu, click Contribution s .

  3. In the Contributions toolbar, select the time span and type of chart you want to display.

  • Meter Processor
  • Meter Processor Charts
  • Consumption Log Calculation