earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Sustainability
Product version: 2024, 7.0
12/10/2024

Consumption Signature Menu

Use the Consumption Signature menu to open and edit general properties and the signal consumption chart.

 
action_zoom_plus_stroke Consumption Signature menu
Figure: Consumption Signature menu

Table: Consumption Signature Menu

Command

Description

Description

Type a description for the consumption signature.

General

Click to view and edit some of the properties of the signature consumption.

For more information, see Consumption Signature – General Tab .

Signature alarm

Connect signature to a new alarm

Click to create a new alarm.

Go to consumption signature alarm

If an alarm is created, click to open the alarm.

For more information, see Consumption Signature .

Signature configuration

Click to configure the signature consumption chart.

  • Consumption Signature
  • Consumption Log Calculation
  • Consumption Signature Configuration Interface WebStation