earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 警报
产品版本: 2024, 7.0
2024/2/23

XLSX Template Tab

Use the XLSX Template tab to configure a template.

 
action_zoom_plus_stroke XLSX Template tab
图: XLSX Template tab

表格: XLSX Template tab

Component

Description

Edit with spreadsheet editor

Click to open the XLSX spreadsheet for editing.

Import XLSX file

Click to import an XLSX file.

Go to report

Click to navigate to the XLSX report.

Generate preview

Preview generated report

Click to preview a generated report including all data.

Preview generated report without data

Click to preview the substitution codes without any data. Use this preview to make sure that the context does not overlap.

Copy to spreadsheet

Displays the substitution code to be used in the spreadsheet. Copy the substitution code and paste it into the spreadsheet where you want to display it.

 
action_zoom_plus_stroke

Add context

Click to add a context to the template.

 
action_zoom_plus_stroke

Edit context

Click to open the Context Configuration dialog and edit the template.

 
action_zoom_plus_stroke

Remove context

Click to remove a context from the template.

Binding data

Click to open the Binding data tab, to add, edit or remove binding data.

  • XLSX Reports Overview
  • XLSX Reports Workflow
  • XLSX Report Template Tab
  • XLSX Template Tab
  • XLSX Report Trigger Settings Tab
  • Context Configuration – Template Tab
  • Context Configuration – Calculation Tab
  • Context Configuration – Misc Tab