earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 警报
产品版本: 2024, 7.0
2024/2/22

Context Configuration – Template Tab

Use the Context Configuration – Template tab to configure the template.

 
action_zoom_plus_stroke Context Configuration – Template tab
图: Context Configuration – Template tab

表格: Context Configuration – Template Tab

Component

Description

Context name

Type a name for the context.

Binding data

Select, edit, or create binding data.

Include column header

Select to include column headers in the report.

Include unit

Select to include the unit you want to include in the report.

Use horizontal layout

Select if you want a horizontal layout.

Use default layout

Clear Use default layout if you want to manually select available properties.

Available properties

Displays available properties that can be included in the report.

Selected properties

Select available properties to be included in the report. Use default layout must be cleared for the properties to be selected.

Copy to spreadsheet

Displays the substitution code to be used in the spreadsheet. Copy the substitution code and paste it into the spreadsheet where you want to display it.

Preview with test data

Displays the data that you have configured.

  • XLSX Reports Overview
  • XLSX Reports Workflow
  • XLSX Report Template Tab
  • XLSX Template Tab
  • XLSX Report Trigger Settings Tab
  • Context Configuration – Template Tab
  • Context Configuration – Calculation Tab
  • Context Configuration – Misc Tab