earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Как

Как


Продукты: Edge Server, Enterprise Central, Enterprise Server, Project Configuration Tool
Функции: Безопасность
Версия продукта: 2024, 7.0
03.12.2024

Activating a Certificate from Windows Certificate Store Using WorkStation

You activate a certificate from Windows Certificate Store if you have stored the certificate there.

Показать больше
action_close

You can use Windows Certificate Store to store certificates used for Enterprise Server and Enterprise Central authentication. In this case you do not use WorkStation for the storage functions. Instead you use Certmgr.exe, Windows Certificate Manager Tool.

However, WorkStation is still used for activating the certificates you want to use.

Certificates with Elliptic Curve Cryptography (ECC cipher / encryption) are supported when authorizing servers in EcoStruxure Building Operation.

Use this workflow to import and activate certificates in Windows Certificate Store.

Более подробную информацию см. Windows Certificate Store for Enterprise Server and Enterprise Central Workflow .

To activate a certificate from Windows Certificate Store using WorkStation
  1. In WorkStation, in the System Tree pane, select the server.

  2. Click the Control Panel tab.

  3. Under Security and Communication , click Security Settings .

  4. In the Security Settings Control Panel, click Certificates .

  5. In the Certificates tab, expand Certificate settings .

  6. Select From Certificate Store .

  7. In the Certificate drop down list, select the certificate you want to use.

  • Windows Certificate Store for Enterprise Server and Enterprise Central Workflow
  • Windows Certificate Store for Enterprise Server and Enterprise Central
  • Certificates Tab
  • Importing a Certificate to Windows Certificate Store
  • Activating a Certificate from Windows Certificate Store Using WorkStation