earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Automation Server, AS-B, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Alarms
Product version: 1.9
10/12/2017

Action Notes

​Action notes are grouped by category, with possible actions that may correct the problem listed in each category. An action note specifies the actions that you used to correct the problem that caused the alarm.

 
action_zoom_plus_stroke Action Notes dialog box
Figure: Action Notes dialog box

Reporting the actions that were taken is either voluntary or mandatory. You can configure the alarm so the user is required to report the actions when certain events occur, such as when an alarm is disabled.

​Action notes can be of great use the next time the same alarm is triggered or when extracting alarm statistics.

  • Alarm Functions
  • Alarms Overview
  • User Actions
  • Alarm Control Panel – Action Notes View
  • Configuring Forced User Action
  • Adding an Action Note to an Alarm
  • Editing an Action Note
  • Creating an Action Note
  • Import and Export of Supporting Objects