earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Edge Server, Enterprise Server, AS-P, Project Configuration Tool
功能: 警报
产品版本: 2024, 7.0
2024/12/3

Adding a Checklist to an Alarm

You add a checklist to an alarm to troubleshoot the problem that triggered the alarm.

显示更多
action_close

A checklist is a set of steps that guides the user to which action to take when an alarm is triggered. If an alarm goes to normal state, the corresponding checklist is also reset and each step has to be checked again.

Checklists can be voluntary or mandatory. You can force the user to check each step in the checklist before the alarm can be acknowledged.

To add a checklist to an alarm
  1. In WorkStation, in the System Tree pane, select the alarm object to which you want to add a checklist.

  2. In the User Action tab, in the Checklist box, enter the checklist you want to add to the alarm.

  3. Click the Save button

     
    action_zoom_plus_stroke
    .

To add a checklist to an alarm, you must have created one in advance and defined its content.

  • Alarm Functions
  • Alarms Overview
  • User Actions
  • Alarm Control Panel – Checklists View
  • Configuring Forced User Actions
  • Configuring Forced User Actions using WebStation
  • Adding a Checklist to an Alarm
  • Adding a Checklist to an Alarm using WebStation
  • Editing a Checklist
  • Editing a Checklist using WebStation
  • Creating a Checklist
  • Creating a Checklist using WebStation
  • Import and Export of Supporting Objects